I have some confusions about the PCB routings of nRF2401.
In the nRF2401 product spec, pins#24, 20 and 17 are connected togther to Vdd. From the Nordic given PCB layout, the routings of these 3 pins seem touching (or passing through) the center pad of the die, which is supposed to be ground, right?
What things should I do in the layout so as to prevent any shorting?