I am using a Blue Smirf to perform a PC → PIC(1) serial connection. Works great! Now I would like to transmit information to a secondary PIC(2) via PIC(1).
Ultimately, I am using a PC to send control variable to PIC(1). Once these variables are transferred the PC is turned off and the PIC(1) controller is left to run remotely. However, I would now like to send monitoring data to PIC(2) that has a serial display.
Since the PC->PIC(1) setup is a bit of a blackbox any help in addressing (literally) the PIC(1) and PIC(2) link. I know that a laipac RF link would do this however, I already have one Blue Smirf and simply want to add one more.