I’ve been using port-o-rotary daily for nearly a year now, and the battery can no longer last a full day on a single charge. After 8 hours or so, even on the first call of the day, the person on the other end reports they can barely hear me, and the ringer barely or not at all rings when it should.
So looks like I need a new battery, and I see this: http://www.sparkfun.com/commerce/produc … ts_id=8484 – this would be pretty keen. Can I use this battery as-is, or do I need to make modifications, and if so, what kind?
On another note, missing DTMF is kindof a bummer, I built a nice bluebox which also does DTMF from http://www.projectmf.org/, but it is quite the task (sometimes 20+ tries) get it to go through as-is using just audio. Seems like typical cellphones do something with the carrier to get a clean DTMF tone through – have you ever had your DTMF tones misunderstood by the remote end due to poor signal? No, they just seem delayed, like a negotiation with the cell carrier is going on. So it seems like I should need to change the firmware to do the DTMF tones for me.
There is also a report that you used to be able to buy the guts of the port-o-rotary separately, but I cannot find it. I wouldn’t feel comfortable making any modifications at all unless I knew I could purchase a replacement logic board. If I screw up, I’ve got to dump $200 on another phone I don’t need… Any chance of this coming back someday?? Hell I’d buy two now for just in case, I want this phone for life.