I recently purchased 2 Postcards along with a LoRa radio to create a GPS tracking system with a base station and a rover. I am configuring my base and rover and had a question. I want to initially do a Survey In and have the results of that survey in to be automatically stored and the base switched to Fix mode automatically so that a power cycle doesn’t initiate a new Survey In. Can someone help? If this is not possible, can this be put on a list to have updated in the firmware? thanks
1 Like
Hi @pauldixon - Your best bet is likely to do the survey-in then record the coordinates using Commonly Used Coordinates. Then switch to Fix mode and select those coordinates. On the next power cycle, the device should boot directly into Fix Base mode.
1 Like
Thanks. Yes, that is what I was planning to do, just a bit cumbersome - ideally it would store these automatically - ie survey in and then switch to fixed with the coordinates.
2 Likes