ZED-FP9 Survey-In Mode

Hello, I am using two ZED-FP9 board as a Base station and a Rover. For the testing I am performing, it is required that we move the base station antenna to different locations throughout the process. The only way we have found to establish the new Base station location is to power cycle the base station. That way when it is powered back on, a new survey is completed to get the new location. Is there a way for the general location to be stored and used to speed up the survey when it is run again?

Any info or tips would be greatly appreciated.

You can typically store the base station’s location information in its configuration or memory. This information can include coordinates (latitude, longitude, and altitude) as well as any relevant geodetic datum. By storing this data, you can avoid the need to conduct a full survey every time the base station is moved to a new location. It can significantly speed up the setup process.

Thanks for the response. Is there a command needed to store the location or does this happen automatically? Also, is there a different configuration mode where it does not conduct the full survey? I am currently keeping the base station in the Survey-In mode. I have not used the fixed position mode yet but that seems like what would be used here.