Postcard RTK - Problems Starting with Firmware v06 LG290

Postcard RTK - Problems Starting with Firmware v06 LG290

Hi @Sparky and @PaulZC.
I haven’t had any success using the Postcard RTK with Portability Shield with the new LG290p firmware v06.
I’ve used combinations of firmware v2.2 and v2.3 with the new LG290 v06 version.
Sometimes it seems to work, but most of the time it gets stuck on the screen with the word Rover.
When installing v2.2 and v2.3, I tried resetting to factory defaults, but I haven’t had any long-term success.
I also noticed that when resetting to factory defaults, port B would change speed to a lower speed than 460800, so Quectel 2.1 wouldn’t receive it correctly.
I also noticed that the option to enable HAS in v2.3 is missing when using v06 of the LG290. Is this true?
Any ideas?
I want to continue investigating Galileo HAS corrections, but I’m stuck because of this problem.
Regards
Angel

Hello everyone.
Any updates on what I mentioned?
Greetings

Hello Angel,

I am away from my desk for a few days. We will try to answer early next week.

Best wishes,
Paul

Thanks, Paul.
Thank you very much and best regards.

Hi @PaulZC and @Sparky

Any news on the LG290P firmware v6 ?
I haven’t been able to test it on the Postcard RTK, as it crashes on startup.
Regards
Angel

Hi Angel (@amlago ),

Apologies for the delay. I am starting to investigate this. My notes so far are in the GitHub issue below.

Best wishes,
Paul