I’m trying to use the Power Delivery Board with STUSB4500 chip. I connected it to arduino and programmed required PDOs (finished with calling write()). When connected to arduino it works fine and negotiates highest priority PDO with the battery. When I try to remove arduino board and use the Power Delivery Board standalone it doesn’t work any more. I’m getting 0V on the VSNK. I checked VIN and there is 5V available. Any idea what I’m missing?
I tried both battery and power supply. Results are the same. Both battery and power supply work nicely with imx8mm-evk board so I assume they’re good. I’m enclosing the pictures of both battery and power supply. I went through the guide you linked. As I wrote before it all works nicely as long as the power delivery board is connected to arduino with I2C. When I unplug, it doesn’t work any more. The MVM values seem to be saved to the STUSB4500 chip. When I plug it back to arduino I can read the values I set. I would expect at least 5V on the VSNK as this is the value in PD0 and it’s supported by both psu and battery.
Hmmmm. I think the power deliver board could be non functional. I apologize for the inconvenience there. I feel as if it should work based off of the data you have provided.
This is unexpected. I was pretty sure I did something wrong. Anyway, I soldered some wires to the board already. I also didn’t purchase directly from you but from The PiHut in UK (https://thepihut.com/). Does the return form still apply in this case?
Hmmm, I would go through PiHut for a return in this case. Just let them know you were working the SparkFun’s support and they should be able to help you assuming you fit their returns criteria.