Issue: cant get output current
Details: Profiles set correctly (15vdc @3amps or 20vdc @3amps)
As soon as I hook it up to anything that would use that power the board cuts output power, either zero vdc or 6vdc (using 20vdc profile).
I will hook this up to a 65watt USB PD charger, the correct profile will be accepted, hook it to a batter charger circuit, then watch as the voltage disappears and it never supply current. I can even hook it up to a usb output device and it supplies little to no output current. (0.1 range).
Even hooking it up to a battery to try and test if it can supply any charging current (albeit no protections) and it killed it.
So im having trouble understanding what this device is for and why it cant pass through the PD currents from the agreed profiles. I wanted to use this to add USB C charging to a GoalZero Yeti150 to charge the built in battery. This Sparkfun board wouldve provided just the voltage and current and the yeti device would’ve took care of the smarts of the charging circuit.