I want to use the Sparkfun Power Delivery Board in order to force an ANKER PowerBank 737 to output power at 12V, with up to 3.0A being drawn from the device. The device is an endge computer which has not capability of negotiating a power delivery contract with the PowerBank.
I used the Example2-SetParameters.ino from the Sparkfun GitHub project
“sparkfun/SparkFun_STUSB4500_Arduino_Library Public”
in order to set the PDO3 values to 12V and 3.0A, like so
usb.setVoltage(3, 12.0);
usb.setCurrent(3, 3.0);
usb.setLowerVoltageLimit(3, 10);
usb.setUpperVoltageLimit(3, 10);
After resetting the Power Delivery Board the yellow LED next to PDO3 lights up. But I am not sure that I am getting that output. How can I force the Power Delivery Board to always output power via PDO3?