Hi Guys, I followed the power supply buildin tutorial, and it lights the light but the voltage reg gets very hot and smokes, i then put the thermistor in and it has to cut the power off every time i turn it on. Have ordered new voltage reg, but why is this happening? photos are on the link below:
Do you have both of the electrolytic capacitors oriented so that their negative terminal is connected to ground? I can’t quite tell from your pictures.
I can’t read the chip, but it looks a lot sleeker than any of the 7805s I have in my stash. A lot of other 3-pin regulators have different pinouts. If you got the wrong regulator, you might have it hooked up wrong. If it’s not a 7805, It’s a good idea to look up the pinout from the datasheet for the exact part number you have.
If the voltage regulator is getting hot and the resettable fuse opens right away, you have a wiring mistake or the chip is defective. Clicking on your link I can only see the first photo, schematic, and parts list. The schematic calls for an ASM1117-x and the first photo shows a TS1086CP-x. Which are you using? I can’t find a datasheet for the ASM1117. The TS1086CP-x datasheet indicates that pin 1 is ground, pin 2 (heat sink tab) is output, and pin 3 is input (pin 1 is the leftmost pin as shown on your photo). Check over the wiring of the regulator and confirm that it is wired properly.