I am trying to power an SS49E hall sensor with a digital pin on the Arduino. When the sensor is directly connected to 3.3V and ground, the signal averages 545 counts with a range from 535 to 555 with North and South polarity which I believe is the correct response. When I power the SS49E with a digital pin, the output is highly variable and never exceed 150. It seems to react to the magnet at times but is very inconsistent.
Ian