pressure sensor for boxing heavy bag

Hi, not sure if this the right place to post this, but - I am interested in embedding pressure sensors in a heavy bag (the kind boxers use) that would send to an app (on an iPad for instance) the location of a strike on the bag, the number of strikes in a specified period of time, and the force that the strike delivered. The objective would be to train the athlete to increase strike force, accuracy and frequency.

I am not sure which products would be most appropriate - at a minimum I would need the pressure sensors and some kind of wireless connection from the bag to the app, and a power source. And the devices would have to be rugged and durable for obvious reasons.

Thanks, Tom

Hi Tom,

I’m not sure if SparkFun will have the right sensors for this project. We have a few force sensors like this [25lb FlexiForce Pressure Sensor that you could, theoretically, install under the surface of the heavy bag but they are not really intended for the kind of abuse that a lot of punches/kicks would cause. Also, this specific one maxes out at 25lbs and I would imagine the strikes will exceed that by quite a bit.

We do have [a similar sensor that has a 100lbs capacity but it has a very small sensing area so it would be difficult to get accurate data without a lot of these placed throughout the bag. The issue with this would be the same as the 25lbs sensor in that they’re not really designed for high-impact applications and may get damaged in this specific project. If you are interested in learning more about the FlexiForce sensors, I would recommend taking a look at their [User Manual.

I hope this helps you determine if SparkFun has the right sensors for this project and if, after reading more about the FlexiForce sensors, you would like to build a prototype circuit, let me know and I can recommend a few development boards that would have built-in wireless capability for you to send the data wirelessly.](https://cdn.sparkfun.com/datasheets/Sensors/ForceFlex/FLX-FlexiForce-Sensors-Manual.pdf)](FlexiForce Pressure Sensor - 100lbs. - SEN-08685 - SparkFun Electronics)](FlexiForce Pressure Sensor - 25lbs (1" area) - SEN-11207 - SparkFun Electronics)