I get this error whil following the instructions posted here …
https://learn.sparkfun.com/tutorials/in … rd-manager
File required seems to be missing … Please tell me how to get past this issue.
Thank you.
Steve
I get this error whil following the instructions posted here …
https://learn.sparkfun.com/tutorials/in … rd-manager
File required seems to be missing … Please tell me how to get past this issue.
Thank you.
Steve
Hi Steve,
This issue is related to a site outage we experienced yesterday (7/31). We are currently investigating the issue and will get it resolved ASAP. Unfortunately, there is no workaround available in the meantime.
When I try to get Arduino Board Manager to install the Artemis, I get an error at the bottom of the screen:
Error downloading https://cdn.sparkfun.com/large /win32_aneg-8-2018_2018-q4-major.zip
Can you suggest a solution, please? Thank you.
A solution may have been reached. Please try installing the Arduino core now and let us know if it works for you.
I can get past the Arduino Board Manager loading the file for Artemis now. Thank you. Unfortunately, nothing complies. I get an error upon attempting to compile any example:
Arduino: 1.8.9 (Windows 10), Board: “SparkFun BlackBoard Artemis, 115200, SparkFun Variable Loader (Recommended)”
exec: “C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major/bin/arm-none-eabi-g++”: file does not exist
Error compiling for board SparkFun BlackBoard Artemis.
This report would have more information with
“Show verbose output during compilation”
option enabled in File → Preferences.
In case this helps, here is the verbose version of the error message:
Arduino: 1.8.9 (Windows 10), Board: “SparkFun BlackBoard Artemis, 115200, SparkFun Variable Loader (Recommended)”
C:\Program Files (x86)\Arduino\arduino-builder -dump-prefs -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\rrobl\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\rrobl\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\rrobl\Documents\Arduino\libraries -fqbn=SparkFun:apollo3:amap3blackboard:svl_baud=115200,loader=sparkfun_svl -vid-pid=1A86_7523 -ide-version=10809 -build-path C:\Users\rrobl\AppData\Local\Temp\arduino_build_223511 -warnings=none -build-cache C:\Users\rrobl\AppData\Local\Temp\arduino_cache_471560 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arm-none-eabi-gcc.path=C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major -prefs=runtime.tools.arm-none-eabi-gcc-8-2018-q4-major.path=C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major -verbose C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5\libraries\Examples\examples\Example0_Compilation\Example0_Compilation.ino
C:\Program Files (x86)\Arduino\arduino-builder -compile -logger=machine -hardware C:\Program Files (x86)\Arduino\hardware -hardware C:\Users\rrobl\AppData\Local\Arduino15\packages -tools C:\Program Files (x86)\Arduino\tools-builder -tools C:\Program Files (x86)\Arduino\hardware\tools\avr -tools C:\Users\rrobl\AppData\Local\Arduino15\packages -built-in-libraries C:\Program Files (x86)\Arduino\libraries -libraries C:\Users\rrobl\Documents\Arduino\libraries -fqbn=SparkFun:apollo3:amap3blackboard:svl_baud=115200,loader=sparkfun_svl -vid-pid=1A86_7523 -ide-version=10809 -build-path C:\Users\rrobl\AppData\Local\Temp\arduino_build_223511 -warnings=none -build-cache C:\Users\rrobl\AppData\Local\Temp\arduino_cache_471560 -prefs=build.warn_data_percentage=75 -prefs=runtime.tools.arm-none-eabi-gcc.path=C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major -prefs=runtime.tools.arm-none-eabi-gcc-8-2018-q4-major.path=C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major -verbose C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5\libraries\Examples\examples\Example0_Compilation\Example0_Compilation.ino
Using board ‘amap3blackboard’ from platform in folder: C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5
Using core ‘arduino’ from platform in folder: C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5
Detecting libraries used…
“C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major/bin/arm-none-eabi-g++” -DPART_apollo3 -DAM_PACKAGE_BGA -DAM_PART_APOLLO3 -c -g -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -fdata-sections -Os -ffunction-sections -w -std=gnu++11 -fno-threadsafe-statics -nostdlib --param max-inline-insns-single=500 -fno-rtti -fno-exceptions -w -x c++ -E -CC -mcpu=cortex-m4 -DF_CPU=48000000L -DARDUINO=10809 -DARDUINO_AM_AP3_SFE_BB_ARTEMIS -DARDUINO_ARCH_APOLLO3 -DPART_apollo3 -DAM_PACKAGE_BGA -DAM_PART_APOLLO3 “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5\variants\SparkFun_BlackBoard_Artemis/config” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/ard_sup” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/ard_sup/ard_supers” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5\cores\arduino” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5\variants\SparkFun_BlackBoard_Artemis” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/mcu/apollo3” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/mcu/apollo3/hal” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/mcu/apollo3/regs” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/utils” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/CMSIS/AmbiqMicro/Include” “-IC:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\hardware\apollo3\1.0.5/cores/arduino/am_sdk_ap3/CMSIS/ARM/Include” “C:\Users\rrobl\AppData\Local\Temp\arduino_build_223511\sketch\Example0_Compilation.ino.cpp” -o nul
exec: “C:\Users\rrobl\AppData\Local\Arduino15\packages\SparkFun\tools\arm-none-eabi-gcc\8-2018-q4-major/bin/arm-none-eabi-g++”: file does not exist
Error compiling for board SparkFun BlackBoard Artemis.