There is a lot of useful information in the post linked below. But I’m guessing you may have already seen it?
Sadly, you can’t test this on the table. The IM19 and GNSS antenna need to be physically coupled together, the antenna needs to be outdoors, and you need RTK Fix. Only when you have all three can you start the IM19 calibration.
Sorry! But that’s just the way it is. ‘Faking it’ with the antenna outdoors and the IM19 in the warm and dry doesn’t work…
Also, please check you are using the correct WORK_MODE. I’m not sure which one is going to be best for your application. Probably 72?