I have problem to upload this sketch to Arduino Uno trough bluetooth. I have tried both 57600 and 115200 baud rate.
#include <SoftwareSerial.h> 
int bluetoothTx = 0;  // TX-O pin of bluetooth mate, Arduino D2
int bluetoothRx = 1;  // RX-I pin of bluetooth mate, Arduino D3
SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);
int led = 13;
void setup() {
  Serial.begin(9600);  // Begin the serial monitor at 9600bps
  bluetooth.begin(57600);
  pinMode(led, OUTPUT);
}
void loop() {
 digitalWrite(led, HIGH);
 delay(1000);
 digitalWrite(led, LOW);
 delay(1000);
}
I’m using following bluetooth module, SparkFun Bluetooth Modem - BlueSMiRF Silver.
It seems to connect but after a while following error message appears and the connection is lost.
Arduino: 1.8.13 (Windows 10), Board: "Arduino Uno"
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 1 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 2 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 3 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 4 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 5 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 6 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 7 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 8 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 9 of 10: not in sync: resp=0x28
avrdude: stk500_recv(): programmer is not responding
avrdude: stk500_getsync() attempt 10 of 10: not in sync: resp=0x28
avrdude done.
Can someone help me with this problem?