Problem using both CC3000 shield and GPS shield

Hello. I am a little new to this so please go easy on me.

I have a Redboard, a CC3000 shield, and a GPS shield with EM-506, all from SparkFun. I can get both shields working on their own with the Redboard, no problem. I can not however get them to work together. I am using the GPS shield in DLINE mode which uses pins 2 & 3 for software serial. I think the problem is that the CC3000 shield uses pin 2 for INT. I was thinking that I could just cut the trace on the CC3000 shield between pin 2 on the header from the redboard and JP2 pin 3. I could then solder a jumper from JP2 pin 3 to JP3 pin 2. JP3 pin 2 goes to redboard pin D9. Then I could change my sketch to use Pin 9 for INT instead of pin 3. Do you think my plan will work? I think so :!:

Thanks!