Hello, i am trying to apply the hello world Example using AmbiqSuite-R2.4.2 SDK with Artemis Redboard
i am using Jlink (PLUS) with IAR/Keil IDE
the programs actully works ,(i tryed many examples with delayes , rtc_isr …) but without any output , i could not see any thing as output
there is nothing from printf funktions and LED0 does not work at all
here is some code:
//printf
am_bsp_uart_printf_enable();
am_util_stdio_printf("Hello World\n");
//LED0
   am_hal_gpio_fastgpio_enable(AM_BSP_GPIO_LED0); 
    am_hal_gpio_fastgpio_set(AM_BSP_GPIO_LED0);
// i have noteced that AM_BSP_GPIO_LED0=10 inthe SDK , i tryed also with value 13 but it did not worked too
i notced also that the arduino SDK is very similar and the code above worked in arduino(with results) ,and it workes with( IAR + AmbiqSuite-R2.4.2 SDK )too but withot any real results
i have to work with IAR/Keil and not with Arduino.
i know it is a very simple question ,
if there is a problem please tell me , or if i have to read something suggest please where to start