Aloha!
I’m having some trouble using AVR-IO-B with the supplied ATTINY2313, AVR-PG1 and PonyProg 1.17h. I can’t get PonyProg to accept Interface Setup. When I click “Probe”, it reports “Test Failed.”
I’m using COM2, and have verified that it works correctly with my JTAG ICE and the AVR-MT-128 (my first purchase from you.)
I’ve verified +5V on pin 2 of the AVRICSP header on the PVR-IO-B board, so power is not the problem.
Should I be using “SI prog API” or “SI Prog I/O”, and should any of the control lines be inverted?
I’ve tried PonyProg2000 as well with the same results. I’m using Windows XP. Any suggestions?
BTW, Spark Fun sent me the AVR-PG1, not the AVR-PG1B.