Has anyone used a USB2LPT to be able to program a BlueCore4, using the schematic above? http://www-user.tu-chemnitz.de/~heha/ba … ex.html.en
I tried this, and got a lot of Blue Screen of Death and no connection. I'm using the express card LPT converter.Zachzor:
Has anyone used a USB2LPT to be able to program a BlueCore4, using the schematic above? http://www-user.tu-chemnitz.de/~heha/ba … ex.html.en
The change of BSoD reduced to nearly zero.
Got a link to the express card you are using ?
I take it your express card uses a high base address ?
Any info is greatly appreciated as I too want to try the circuit on a computer with no lpt port.
nicolasg:
Got a link to the express card you are using ?I take it your express card uses a high base address ?
Any info is greatly appreciated as I too want to try the circuit on a computer with no lpt port.
http://www.willtek.net/images/ExpressCard/EXP12.html
I’m sure it will work because I’m using it now.
I think any card with OXPCIe952 will.
Does anyone know the pinout for the RJ45 (SPI) side of the CSR
M1616 USB to SPI programmer?
Sometimes when I try to bef
Hi,
Since about week I’m developing bluetooth modules for my design. But what I want to do is: to programm CSR BlueCore4 chip with example program from BlueLab4.12 (RFCOMM_A and RFCOMM_B or SPP_DEV_A and SPP_DEV_B). But now I’m using these:
http://www.austartech.com/resourcefile/2009245843.pdf
modules and thats what I’m programming. I have two of them. And everything goes ok but when I’m startign to RUN program from BlueLab I have info from debug section (those printf in application code) which is telling me that my devices didn’t see each other. Where’s the problem? Maybe in PStool i have to change some options? Now i used default ones. I have also a Casira development kit but I’m waiting for new modules with BlueCore4 chips onboard because the old ones had BlueCore2 chips and were too old.
Regards