proj about 12f675 in picket1 and nrf24L01,have problem

I just began to study program in asm,and try to code like that, right or not? have some example code for me?

LIST P=12F675, R=DEC

INCLUDE “p12f675.inc”

#DEFINE AA GPIO,0

#DEFINE SCK GPIO,1

#DEFINE CSN GPIO,2

#DEFINE MOSI GPIO,3

#DEFINE IRQ GPIO,5

ORG 000H

NOP

CLRF GPIO

BSF STATUS,PR0 ;choose bank1

movlw b’11000001’ ;GP0-input, GP1-Output, GP2-outut,GP3- outut,GP4-outut, GP5-output

MOVLW TRISIO

movlw b¡¯11001000¡¯ ;Pull Ups Disabled, Rising Edge, Assigned to WDT , Prescaler is 1:1 WDT

movwf OPTION_REG

clrf ANSEL

BCF STATUS,PR0

CLRF STATUS

CLRF INTCON

CLRF GPIO

MOVLW 07H

MOVWF CMCON

CHECK

BTFSC GPIO,0

GOTO CHECK

CALL DELAY

call GetData ; read data

call SendData ; send data

goto main


GetData

return


SendData

return

While it’s definitely a good thing to be familiar with assembly language, I wouldn’t recommend starting there. I use Microchip’s C18 C compiler as there is a free student version (the only limitation is that you can’t use some optimization after 60 days). The only catch is you have to use a PIC18 chip (it won’t compile code for the PIC12 chips). Do you have any prior programming experience in higher level languages?

On my website (see in my tag line below), I have quite a few tutorials on getting the 24L01 working with the PIC18F452 using C18. All the code is on the site, as well as a write-up to explain background material. Don’t forget you’re also going to need a hardware programmer for any PIC you choose as they don’t ship with any type of bootloader installed.