Hi my name is samuel im from dominican republic and im working on this project:
im gonna use a touch LCD as a menu and i will use ethernet so send the selections
on the menu to the computer so i need 3 things:
- 
Arduino (Arduino Mega 2560) 
- 
Ethernet Module (Arduino Ethernet Shield) 
- 
Touch LCD 
i have some problems choosing the LCD but i think i found the one im gonna use
2.4" TFT LCD Screen Module: ITDB02-2.4 with ITDB02 Arduino MEGA Shield v1.1
but i still got a problem looking at the Shield for the LCD i see i ocupies all the ports
from the arduino but it doesnt used them all so im think im putting the Ethernet module
firs cuz it has long wire-wrap and This keeps the pin layout intact and allows another shield
to be stacked on top
i havent started this id like to hear in this cases read some opinions about it