PWM from 3.3V to 5V - BOB-12009

Hi,

I need to boost a PWM signal from 3.3V to 5V to control a servo.

I use BOB-12009 ( SparkFun Logic Level Converter - Bi-Directional - SparkFun Electronics ) but it appears that the HV output low level is shifted at ~1.1V.

I can confirm that LV low level is 0V. Then the servo is not controlled and I can read in its datasheet that low level is expected to be under 0.4V.

High levels are good (+3.3V for LV, and +5V for HV).

Am I doing something wrong ?

Hi @bagelfly ,

BOB-12009 works best in applications like I2C where: a logic high is created by the pull-up resistors; and logic low is created by the controller and peripheral pulling the signal to GND. The circuit comes from an NXP Semiconductors / Nexperia Application Note AN10441.

It does not work well in applications where you need the level-shifter itself to pull / drive an output high and low.

You may need a different solution…

The SparkFun Opto-isolator Breakout would work well. The transistors on the HV side would guarantee the servo PWM signal is pulled to HV-GND (HVG) for logic low.

I hope this helps,
Paul

Hi @PaulZC ,

Thank you for quick answer !

The BOB-09118 seems better indeed. Do you know what is the reference of the transitors Q1/Q2 to deeper check the behavior ?

@bagelfly

They are standard NPN transistors: MMBT2222A

Best wishes,
Paul

That definitely works !

Thank you @PaulZC