Hi…
I saw that to use the ArduPilotMega and IMU Shield [and GPS etc…] successfully with a quadcopter setup, you need this Power Distribution Board setup yet I cannot find it anywhere. It is not available. Is this still needed or was this eliminated in a revision to the boards?
Thanks … trying to sort this all out…
Marc
Marc,
-
What, precisely, is “this Power Distribution Board setup”?
-
I encourage you to read [this guidance before you respond.
Eric](http://forum.sparkfun.com/viewtopic.php?f=14&t=27089)
Marc,
- As odd as it may seem to you, I pointed you to that guidance because it appears that you would benefit from it, specifically: http://www.catb.org/~esr/faqs/smart-que … #beprecise.
- How about starting your quest for help here by providing a link to whatever it is you understood to say a "Power Distribution Board" is necessary for quadcopters but not "a standard aircraft"?
- Why are you asking us instead of the Arducopter folks who referred to a subsystem you can't find?
- Why, if at all, have you rejected the possible interpretation that you need a "Power Distribution Board" because a [[quadcopter](http://en.wikipedia.org/wiki/Quadcopter) has four motors or engines, each of which must be "throttled" independently, but a "standard aircraft" is powered by a single motor or engine?
- I have no experience with either of the ArduPilot boards, but it seems unlikely that either of them can handle the power necessary for flight, so some other device will need to take each motor speed control signal and modulate power to a motor based on it. (That's for an electric-powered craft. For a combustion-powered craft, you might well be able to use a signal from the ArduPilot directly to drive a throttle solenoid.)
- How did you search for the Arducopter PDB? Just for my own amusement, I thought I'd poke around a bit. It took me only a few minutes to find my way [[here](http://code.google.com/p/arducopter/wiki/ArduCopter_Electronics), from which I was able to get to the artwork for the board and assembly photographs. (The link to someone alleged to be selling the PDB (other than in a kit) does, I concede, appear to be broken. That [[company's website](http://fahpah.com/Welcome.html), though, does appear to respond, so you could e-mail them and ask.)
- Based on what I found, the PDB appears to be nothing other than a wiring board, so I don't see why it would be required. It might, however, be the most convenient way to distribute power for such a vehicle.](http://fahpah.com/Welcome.html)
Eric](Google Code Archive - Long-term storage for Google Code Project Hosting.)](Quadcopter - Wikipedia)
Marc,
As you appear inclined to misquote me (I did not, for example, say I “dont know anything about the Ardupilot board”.) or repeat things I’ve said as if you were adding information to the discussion, I hereby respond to the only question in your OP:
fxmodels:
Is this still needed or was this eliminated in a revision to the boards?
monosyllabically: [mu.
Eric](mu)
my 2 cts., but I can understand fxmodels frustrated reaction here.
E
Yeah I see the link to buy the PDB is broken. Looks like someone posted in the comments and got a response w/ link:
http://store.jdrones.com/product_p/quadpdpcb1.htm
The PCB files are available… you could always fab your own if it’s not too hairy of a layout.
Michael
Fxmodels,
Just another 2cts. I am not a moderator either :roll: , but I can say the “welcome message” you received doesn’t reflect the global forum spirit.
Probably someone forgot that not every member is an electronics engineer, nor a good editor when trying to express ideas and thoughts.
Angelo
I don’t see tremendous value to that “Power Distribution Board”. It appears to just provide a way to connect a bunch of ESCs with power and with the signal wires from the ardupilot. I’d suggest changing the original “need” requirement to “nice to have”.
Here’s a picture of the PDB all hooked up:
http://ardupilot-mega.googlecode.com/sv … APM_RC.jpg
Hello guys…
First… Thank you for the great help here. I very much appreciate your kind words and your advice.
It does appear that the PDB is just a cleaner way to do the task over what could be a cumbersome wire harness. If we were to use one it would have to be remade with much thicker solder traces for higher current draw I think. The artwork is available though as some of you have pointed out so this possibility is clearly doable.
Thank you again for the help!
Marc
FX Models
Chagrin:
I don’t see tremendous value to that “Power Distribution Board”. It appears to just provide a way to connect a bunch of ESCs with power and with the signal wires from the ardupilot. I’d suggest changing the original “need” requirement to “nice to have”.
Here’s a picture of the PDB all hooked up:
http://ardupilot-mega.googlecode.com/sv … APM_RC.jpg
Point well taken! Thanks…
Fxmodels:
There are several advantages of using a PDB, the most important one is that
By not using so many wires, you help eliminating electromagnetic interference to the quad copter digital compass. A wiring harness can drive the compass crazy very easily
http://www.mikrokopter.com/files/KompassDreht.wmv
Also, not having a PDB can lead to a messy signal and power distribution where many failures can arise, like desoldered joints, etc…
Using a PDB helps in making room for other components like GPS, video transmitter, on screen display, etc…
Maintaining a quad copter with a PDB is MUCH easier
Assembly is much faster.
So my recommendation is : use a PDB
And lastly… I cannot resist saying that I am sorry to see that your first experience on this forum was with someone that clearly belongs somewhere else and evidently ignores what a PDB is for and couldn’t even find out about it and finally attacked you.
I just prefer to say: welcome!
^^^^^^^^^^^^^^^^^^^^^^^^^^
A few cases of “need to grow a pair” above