About this wireless module.
http://www.sparkfun.com/commerce/produc … ts_id=8250
My application is very space constrained.
Only 41.8 mm space from the top of the microcontroller board.
I need to put this wireless module in right angle from the top of my board (not using the included ribbon cable).
On the product page shows that this module is 34x18 mm.
If the 34 mm length doesn’t include the connector, it’ll not fit on my board(34+8.75 = 42.75).
Can anybody measure the dimension of the board including the connector ?
Thank you very much.