im trying to figure out the dimensions of the qwiic openlog. i intend to purchase one, but i want to make sure it fits onto my project before i do. i was able to find the dimensions for most other products in the sparkfun hookup guides, but not this one. i just need the height, width, and distance between the holes. thank you
Do you use Eagle software? If yes, you can find the dimension from the .brd file given here: https://cdn.sparkfun.com/assets/f/5/a/9 … penLog.zip
no i do not. and i am running this project thru a school, so im not able to download it either
I have one.
Not sure how precise you need it but, looking at the board with the Qwiic connectors left and right and the soldering points GND, 3V3, SDA, SCL at the bottom. No headers applied :
Board size Left to right : 26 mm ( no connectors attached).
Board size bottom to top: 27.4 mm
Center of the hole left to center of the hole right: 21 mm
Diameter holes: 3.3 mm
Distance center of holes from the bottom of the board: 24 mm
Height: 6.6mm
P.s. Please be aware the QWIIC Openlog is different than the Artemis Openlog. The QWIIC Openlog is only to store and retrieve data from a MicroSD. The Artemis Openlog extends that by supporting many sensors
thank you so much. this was exactly the dimensions i was looking for