Qwiic Connect for ZED F9P GPS with Neo D9" and ESP32 Thing Plus

Hi

I’m in the UK, trying to set up a surveying kit with the above products connected via the Qwiic system.

Following the Sparkfun Hookup guide I am having no luck in configuring the kit within Arduinl. I have obtained the L band keys from Thingstream and also tried following the guides provided from Ublox all without success.

Firstly, am I using the correct boards? Is the ESP32 capable of processing data from the Neo and F9P?

Secondly I’m not sure how to set up the I2C ports to transmit from the Neo to the F9P and forward the correction data.

I am a complete novice at this, but it seems very complicated.

I had tried to set up a base and rover configuration, but have managed to overheat another F9P board, which is now scrap on the bench (ouch).

All in all, it has been quite a frustrating and costly exercise so far without any progress.

Any general advice, or example code would be welcome.

Many thanks, Gary

You can, though it will matter a bit on how you’re using them - Which D9S board are you using (combo board w/ F9P or standalone?)