Hi the qwiic glove has a tutorial but items are missing or have been retired
Can someone give me a list of what is needed?
I am not sure they are all needed so if u can make a list that would be great
Hi the qwiic glove has a tutorial but items are missing or have been retired
Can someone give me a list of what is needed?
I am not sure they are all needed so if u can make a list that would be great
Any arduino board with a qwiic port Arduino Boards - SparkFun Electronics will work, with a qwiic cable (in the guide)
There are only 2 retired items, both photons devices…just skip those and the rest of the guide still applies ![]()
Hi
Does that mean you need to buy every single item on the page and u should be good?
Hi so there are two microcontrollers
I chose one and then one shield
I got two SparkFun qwiic flex glove controller
One wire
Where is the power pack so I can power it?
Also the SparkFun RedBoard - Programmed with Arduino - is this microcontroller enough or do I need another arduino?
No, just one MCU, get one that has a qwiic port so you don’t need the shield
Then hook it up like so Qwiic Flex Glove Controller Hookup Guide - SparkFun Learn but using the included onboard qwiic port of your MCU
get 2 qwiic cables if you are getting 2 glove sensors
You can power it over USB with apower pack, or barrel jack Barrel Jack Extension Cable - M-F (6 ft) - COM-11707 - SparkFun Electronics or a 9v from barrel jack 9V to Barrel Jack Adapter - PRT-09518 - SparkFun Electronics …you have a lot of options