My Project includes:
SPX-16282 BlackBoard C
DEV-15165 Qwiic MP3 Trigger
BOB-15931 Qwiic Button Breakout
SPX-15586 Qwiic Switch
My intent is to trigger MP3 sound files, though a group of 18 arcade style switches split into 2 smaller groups of 9
on panels on either side of a screen like on a Battleship style game |
My understanding is that 4 of these switches can be soldered directly to the MP3 Trigger, but how do I connect the other 14 switches physically ?
Option A:?
Connect two of my Arcade buttons to the BOB-15931 Button Breakout board, and one to a SPX-15586 Qwiic Switch,
and daisychain these three together, making three sets of three switches.
To look something like this:
/Button Breakout===Button Breakout===Qwiic Switch ( 3 arcade switches)
BlackBoard C==MP3 Trigger=== -Button Breakout===Button Breakout===Qwiic Switch ( 3 arcade switches)
\Button Breakout===Button Breakout===Qwiic Switch ( 3 arcade switches)
how do I connect these 9 switches to the MP3 Trigger?
Do I need to add a BOB 16784 MUX Breakout beyond the MP3 Trigger to attach the 9 switches and change each address?
Can 3 Button Breakout boards be daisy chained into a single Qwiic connection on the MUX breakout board?
Or do I need to use 2 of the BOB 16784 MUX Breakout boards, connecting 1 arcade switch to 1 port connection on the MUX individually . to make 16 connections and can use 2 solder connections on the MP3 board for a total of 18.