Qwiic MP3 Trigger - use it although retired or good alternatives?

Hi there, I use several Qwiic devices in a prototype.

To add audio I consider testing the Qwiic MP3 Trigger. But I see that is is retired and I did not find an indepth test of the device (stability, reliability..).

What I need:

  • reliable and repeatable playing of short audio clips (like 200ms “fire” and “reload” effects)
  • either WAV or MP3, doesn’t matter (I assume from past projects that WAV would suit more as it does not need the same processing power as MP3 to play)
  • small form factor
  • connection exclusively via Qwiic (as RX/TX is already used for a 9DOF IMU INT/RST signal)

As board I use a MicroMod SingleSlot with ESP32, the MicroMod slot is already used for PoE Ethernet.

Alternatives I’ve found:
SparkFun Serial MP3 Player Shield - MY1690X-16S (Qwiic)

  • that one seems to be the closest alternative as it has Qwicc (but only 1), Jack and SD Card
  • but the size is a bit big
  • does this work soley with Qwiic or does it need an TX/RX connection too? In the hookup guide Pinout section it mentions TX/RX but I am unsure if that is optional or a requirement; in the Git Repo I only find examples for Serial communication)

SparkFun Qwiic WAV Trigger Pro

  • seems to be the more expensive and most recent version of the one above?
  • it has 2 Qwiic which is good
  • it has an SD Card slot (on the backside)
  • I understand that it would need an TRRS 3,5 Jack breakout board for headphones
  • or what would I need to use to connect a speaker instead of headphones? (Just solder the speaker to the pinouts?)

SparkFun Audio Codec Breakout - WM8960 (Qwiic)

MP3 Trigger

  • too big, no Qwiic, expensive

Tsunami Super WAV Trigger (Qwiic)

  • too big, expensive

SparkFun Qwiic Buzzer

  • maybe as fallback solution for simple noises

SparkFun Audio Player Breakout - MY1690X-16S

  • no Qwiic

SparkFun Qwiic Speaker Amp

  • that is just an AMP, right?

My questions:

  • which Qwiic alternative would fit best for the scenario? Did I miss an alternative? Or should I go with the Qwiic MP3 Trigger first?
  • I’ve had severe issues with another audio chip in the past (DFRobot DFPlayer) with issues like crashes when rapidly playing audio files after each other (intervals <200ms), random lockups, cracks and noises.. I couldn’t find an “indepth” test of the Qwiic MP3 trigger but was wondering if someone has experiences or if maybe there are similar issues that lead to the retirement (I’ve read some postings here in the forum about noise and hookup problems)

I think SparkFun Serial MP3 Player Shield - MY1690X-16S is good for you. SparkFun Serial MP3 Player Shield - MY1690X-16S (Qwiic)

I agree with dilshana; it has both serial and i2c (although we don’t have an example for i2c, it seems) https://cdn.sparkfun.com/assets/5/4/5/3/0/SparkFun_Serial_MP3_Player_Shield_MY1690X.pdf

Thank you for your reply.

Unfortunately I cannot find the DEV-28021 Serial MP3 Player Shield at any distributor to order.

Is DEV-28021 something very new or special that can only be ordered at Sparkfun directly (part: 15$, shipping: 100$ .. not so great) ?

I’ve tried:

  • Digikey (where I usually order Sparkfun stuff as they have most parts available)
  • Mouser
  • Amazon
  • BerryBase
  • Distrelect
  • Robotshop
  • Reichelt (German distributor)
  • Conrad (German distributor)

I will try the WAV Trigger Pro first at it is available at Digikey.

Did you search at RS components?

It is an older product, I’d guess those distributors simply didn’t sell enough to justify re-stocking :-/

Also be sure to check ebay!

Hi @TS-Russell , I see that the Git Repository started in January 2025 and there have been several commits since then, the last 2 months ago.

Is it really an old product? Maybe you mistake the SparkFun Serial MP3 Player Shield with the 10-year-old SparkFun MP3 Player Shield ?

Ah, I did have them mixed-up! Oddly this might be the exact opposite situation I described above, it’s a bit newer and some distros only order every 3-6 months so some might not have it stocked/ready yet :-/

Sorry about getting them confused!

Which country are you in?

Hi, sorry forgot to reply - I am in Austria.

RS components does not have it.

The only supplier I have found is Digikey
, but with a lead time of 10 weeks.

@TS-Russell do you see any other option?

I found a supplier in one of Austrias neighbour countries (Slovakia) that has it in stock.

For anyone else in my situation, its available here:

Nice! Good work

Update:

I received the device, but unfortunately the Serial MP3 Player Shield might not meet my requirements. At least from the examples and hookup guide, the board needs serial communication.

In the hookup guide, there is no part about using Qwiic.

On the Github repo I found an example labeled QwiicTwist but it is using I2C to connect to the Qwiic Twist and uses serial communication to control the MP3 Player Shield.

In the examples or SparkFun_MY1690_MP3_Library.h I couldn’t find any reference to Wire, I2C or Qwiic.

@TS-Russell you mentioned earlier that there is no Qwiic example. Is it just that the example is missing (could you ask to provide one?) or is it not possible to control and use the Serial MP3 Player Shield only via Qwiic?

The Qwiic port on the shield is connecting other devices, it’s not for actually controlling the shield. You need TTL serial to control the shield. It is not possible to control the shield with Qwiic.

Oh ok.. thats too bad. Then I have to go with Wav Trigger Pro being the only option here that works only via Qwiic.

For everyone else coming here, in the end I solved it by using the Wav Trigger Pro along with a modified firmware (half clock speed, lower temps) + the Qwiic Amp - works perfectly along with other Qwiic devices.

Read more here: WAV Trigger Pro - runs a bit hot - #15 by michaelheiml82