I am making a prop weapon and am using a qwiic mp3 trigger board. I have no issues with getting it to play regular single or multi shot sound files. But when I try and play a short file of a full auto shot sound while holding down the trigger it sounds like it is only playing the center of that short mp3 and there is also a very noticeable delay between playing while using the built in triggers. I tried making a 6 shot loop file as i thought it might just be the very short mp3 of a single shot of full auto it didn’t like but there is still a very noticeable delay between repeats while holding down the trigger.
I messed around with it hooked to a redboard with qwiic wire and played the sounds from the example tht has the serial monitor menu but have seen much the same results.
Am I doing something wrong or is this board not going to work for my project?