Hello,
I bought two QWIICc Quad Solid State Relay (part number: 16833, link: https://www.sparkfun.com/products/16833)
I also bought four: Qwiic Cable - Breadboard Jumper (part number: 14425, link: https://www.sparkfun.com/products/14425)
I would like to control these relays with a Raspberry Pi 4, but I cannot get it to work. My problems is exactly the same to this topic: viewtopic.php?f=105&t=55721
When I connect the Raspberry pi to an Adafruit PCT2075 temperature sensor (I2C), and I run i2cdetect, it gives confirmation that the 0x37 adress (as expected) is connected. Therefore the I2C is correctly configured.
I followed this tutorial for configuring I2C (https://www.artekit.eu/enabling-the-i2c … pberry-pi/)

However when using the SAME Raspberry Pi, connected the SAME manner, running i2cdetect, nothing is detected. This is the case for both Quad relays (16833). The power led on the board is lit, showing it receives power.

I connected the Raspberry Pi in the following manner to the breadboard jumper (14425):
3.3V to red cable
GPIO 2 (SDA) to blue cable
GPIO 3 (SCL) to yellow cable
GND to black cable
I also switched the SDA and SCL to no avail.
Do I need to use an external power supply? Or can I connect the red cable to a 3.3V pin of the Raspberry Pi? What can I do to get this working?