Hi,
The MCP9600 Qwiic Thermocouple Amplifier (SEN-16295) is a supported device with the IOT datalogger.
When the MCP9600 is connected to the IOT datalogger it does not show up as a connected device, under the device setting selection.
I’ve tried with two MCP9600 boards and neither show up, I’ve also tried with the IOT-9DOF datalogger, same result.
When either MCP9600 is I2C scanned using a MicroMod micro it shows up as hex address 0x60, the default.
Please advise if this is due to a software version or some other issue or should the I2C address be different?
The datalogger firmware shows as Version: 01.00.03 - build 000099
Please advise Ronald Ross