hello everybody,
i have two xbee series 2 of the Digi, linked to the PC with this board: http://www.robot-italy.com/product_i…roducts_id=742
i’m using x-ctu ad put into them firmware in API mode and tried to perform a range test, but it doesn’t work.
what’s the problem? is possible to perform a range test with API mode?
i tried also to send a packet from the coordinator to the second module (router/end device), but nothing is happen
es: 7E 00 0A 01 01 13 44 00 48 65 6C 6C 6F B8
or: 7E 00 12 10 01 00 13 44 00 40 4A 50 7E 13 44 00 00 63 69 61 6F C3
thanks
Nichis