Hello,
After connecting the “Magnetic Imaging Tile - 8x8” to 3,3V the voltage of my micro controller dev board (esp32) breaks down immediately. It looks like a short, but i cant find any on the “Magnetic Imaging Tile - 8x8” board. The resistance between 3,3V and Grd pin is 20k Ohms. One chip (sn74lvc1g139) is getting hot fast, while voltage is applied. Now I am quite worried, that the module is broken. I could go on testing connecting all other SPI and analog out pin, but I doubt that hot chip will cool itself down again. I will try on a arduino nano with 3,3v and let you know.
Optical inspections and electrical inspections did not show any faults so far. I could not check for correct orientation of the chips, because i did not find the marks in the datasheets.
Are the modules tested?
Best wishes, Julius