Ok, I just watched the Kickstarter vid and I don’t see how you will integrate a pump in place of a servo… So, please explain… What is the voltage on the bot, 5V? If so, you will need another power supply that can output 12V, and then setup up a circuit to drive the motor when needed.
So instead of servos with winches pulling wires, you want to use waterflow to move something? The parts I’m missing to make this work are plungers and tubes. Or else it’s going to be a real aquarel painting. Please explain better how you are trying to set this up.
[edit]Dammit, it’s not even a waterpump but a vacuum pump. Now I am really lost.
I’m surprised as well. You’d figure most that would bother posting here would be avid enthusiasts and the number of 1 & 2 post users wouldn’t be so high. Apparently not.
Of course I realize most of the zero posters are people that tried to jump in on the holiday freebie deals, and the single posters are spammers or people that asked questions and didn’t give out a thanks after an answer was thrown out there. Possible that the double-post types asked a question, got an answer and threw out a thanks.
skimask:
Of course I realize most of the zero posters are people that tried to jump in on the holiday freebie deals…
I don’t see how this is possible, the main site and the forums don’t have synced logins. You have to register for the forums even if you have an account on the main site.
codlink:
I don’t see how this is possible, the main site and the forums don’t have synced logins. You have to register for the forums even if you have an account on the main site.
Ok, maybe not... I was making an uneducated guess :)
At any rate, bunches of the registration dates line up with those freebie days, at least within a few days beforehand.