I just received the real time clock module based around the DS1307 and it appears to be dead on arrival. The I2C interface is non-responsive to clean looking read/write commands (slave address 0x68). When I probe the X2 oscillator pin, there is only DC out (not oscillating). I’m assuming that I should see some activity on that pin if the oscillator circuit within the chip is functioning properly.
The battery measures 3.0V so it looks good. I took the crystal off the board and tested it in a test circuit I built. It resonates at 32.768kHz as expected. That pretty much leaves the IC as the issue.
All this testing was done with a 5V source connected to the board.
Does anyone have any other suggestions for troubleshooting before I open a return request?