I am trying to get a SparkFun weather shield running on a RedBoard Artemis. I am using Arduino 1.8.19 and the sample weather shield sketch. I have tried other sketches but none work. Therefore I went back to the simple sketch for the weather shield. Here is the error:
Weather Shield Example
++ MbedOS Fault Handler ++
FaultType: HardFault
Context:
R0: 0
R1: C0
R2: 10001058
R3: A3009150
R4: 0
R5: 1
R6: 0
R7: 0
R8: 0
R9: 0
R10: 0
R11: 0
R12: 18
SP : 10006FB8
LR : 114A3
PC : 12564
xPSR : 41000000
PSP : 10006F98
MSP : 1005FF70
CPUID: 410FC241
HFSR : 40000000
MMFSR: 0
BFSR : 82
UFSR : 0
DFSR : 0
AFSR : 0
BFAR : A3009150
Mode : Thread
Priv : Privileged
Stack: PSP
– MbedOS Fault Handler –
++ MbedOS Error Info ++
Error Status: 0x80FF013D Code: 317 Module: 255
Error Message: Fault exception
Location: 0x12564
Error Value: 0x10005FB8
Current Thread: main Id: 0x100043C0 Entry: 0x242B5 StackSize: 0x1000 StackMem: 0x10006018 SP: 0x10006FB8
For more info, visit: https://mbed.com/s/error?error=0x80FF01 … FE_ARTEMIS
– MbedOS Error Info –