Redboard Artemis not showing up on BOARDS in Arduino Program. COM PORT IS showing up !

I just purchased the Arduino Redboard Artemis as an upgrade from my Arduino Redboard Uno and cannot get the board to appear in the “Boards” section of my Arduino program.

I have installed the CH340 drivers and am successfully receiving the USB-Serial CH340 in my Device Manager. I have tried this on both my Macbook Pro and my Windows 10 PC but am unable to ever see the Arduino Artemis listed under boards. I did not have this issue with my Arduino Uno.

Do i just need to keep troubleshooting it?

Can you confirm that the board manager has the Apollo3 board libraries installed? https://cdn.sparkfun.com/r/600-600/asse … nstall.jpg

I am seeing the same problem on MacOS 10.15.6 – I see the port but not the board.

its still works, but the loader takes time to start… sometimes it doesnt.

I am using 1,2.0 of the Apollo 3 board library

You could have a conflict in the board manager. I’ve seen this happen with our ESP32 board definitions, which is part of the reason why we handed that of to Espressif. Essentially, the Arduino IDE couldn’t handle multiple definitions of the same board (from SparkFun and Espressif) and even if the board definitions were installed, they might or might not show up in the list of boards. Often, this would occur for users with multiple versions of the Arduino IDE.

The only way I was able to easily resolve the issue was to uninstall the Arduino IDE and manually delete the folder containing the board definitions… aka go for a clean slate. It sounds like this could be a similar case.