HELLO,
When I try to upload any sketch to the RedBoard PLUS the following occurs: The program compiles then the “uploading” message appears. The TX Led flashes, the RX does not flash. I then get an error message. I tried a different USB-C cable with the same result. I tried the other PORT with the same outcome. On the Arduino IDE I have “UNO” selected. I have a selection of PORT 2, 5 and 6. I tried them all. I installed an MEGA 2560 and all the programs I loaded compiled, uploaded and worked.
The Power Light is on constantly.
The pin 13 Led flashes blue every few seconds constantly.
The TX LED flashes green about every 3 seconds constantly
The RX never lights up of flashes.
Can anyone please help?