Regarding Integrating Micro LiDAR Module (SEN 15179) and SparkFun GPS Breakout NEO-8MU (GPS-16329)

Dear Forum Members

Can I integrate Sparkfun’s TFMini Plus-Micro LiDAR Module (SEN 15179) and SparkFun’s GPS Breakout NEO-8MU Module (GPS-16329) using Quiic red board such that distance from LiDAR and position values for GPS Breakout can be fetched in the synchronized manner? If it is possible then convey me which Quiic red board is suitable in this case.

Regards

VS (vsinghce)

What do you mean “…in the synchronized manner?” ?

What I mean from “synchronized manner” is that data from the sensors must be sampled at a given time stamp (may be GPS Timestamp) and saved as a row in a file.

Technically, you can call functions to get that data to sample as quickly as possible per timestamp. There are always delays but it’s on the matter of usually fractions of microseconds. I would suggest the following boards:

https://www.sparkfun.com/products/15123

https://www.sparkfun.com/products/15444

https://www.sparkfun.com/products/14713