Revely RMS-100 board doesn`t work

Hi everybody.

I bought a RMS-100 board from Revely a few years a go, and never use it, it´s base on a Sharp LH75401 arm core. I try to load a sample program that comes with Crossworks, specialy written for that board, and doesn´t load. I have to say that the board comes with a program call speedloader v. 1.3, in order to use it you have to load a file with ELF format. The question is what i´m doing wrong when I try to load the file the program send me this errors and don´t load anything.

File Sections

.vectors : 60 LMA bytes outside Flash at 0x00000000 !!!

.init : 596 LMA bytes outside Flash at 0x0000003C !!!

.text : 184 LMA bytes outside Flash at 0x00000290 !!!

.heap : 1024 bytes ignored

.stack : 1024 bytes ignored

.stack_irq : 256 bytes ignored

.stack_fiq : 256 bytes ignored

.comment : 36 bytes ignored

.shstrtab : 92 bytes ignored

.symtab : 2000 bytes ignored

.strtab : 1955 bytes ignored


Errors !!! Press any key.

Thank you for advance

Regards[/quote]