Problem with LPC-E2214 board and LPC2000 utility

Hi all,

my problem is the following:

if i run LPC2000 Flash utility (by Philips) and i try to read the RAM buffer i

always obtain the error ‘Cannot communicate with test board!’ and i see into the buffer only range 0x4000.0000 - 0x4000.384 filled with a (maybe) random values (?).

Why i’m not able to read the whole RAM buffer (size=0x4000) ?? :evil:

If i write my hex files with LPC2000 or lpc21isp utility i never see the code running well: a sample downloaded with IAR environment and JTAG WIGGLER cable is ok.

Thanks !

–

SM

Hi all,

i uploaded the sample H2214_Board_Test.hex on Flash by LPC2000 utility and it is working.

But if i upload the debug version (RAM version, file renamed from .a79 to .hex) by LPC2000 + “RAM buffer operations” dialog, i see only ‘BOARD TEST’ but the LCD did not blink and the final strings are not shown.

My question is: when i load the code the LPC2000 warns about possible code between 0x4000.0120 and 0x4000.01FF. My idea is that this sample has a code in that range (i see a 0x4000.0040 value at address 0x4000.0020) ! The bytes in that range are ignored and then, of course, i have the bad work !

What do you think ?

PS: Again, if i read the 0x4000.xxxx range by ‘Download RAM’ command, i receive the ‘Cannot communicate with test board’ and the data changed in the range 0x4000.0000 - 0x4000.0384.

Thanks !

Anyone own the xcl for IAR compiler + RAM compilation + LPC-E2294 board ?

I modified an existing file and this is the result:

//*************************************************************************
// XLINK command file template for EWARM/ICCARM
//
// Usage:  xlink  -f lnkarm  <your_object_file(s)>
//                -s <program start label>  <C/C++ runtime library>
//
// $Revision: 1.1 $
//*************************************************************************

//*************************************************************************
//
// -------------
// Code segments - may be placed anywhere in memory.
// -------------
//
//   INTVEC     -- Exception vector table.
//   SWITAB     -- Software interrupt vector table.
//   ICODE      -- Startup (cstartup) and exception code.
//   DIFUNCT    -- Dynamic initialization vectors used by C++.
//   CODE       -- Compiler generated code.
//   CODE_I     -- Compiler generated code declared __ramfunc (executes in RAM)
//   CODE_ID    -- Initializer for CODE_I (ROM).
//
// -------------
// Data segments - may be placed anywhere in memory.
// -------------
//
//   CSTACK     -- The stack used by C/C++ programs (system and user mode).
//   IRQ_STACK  -- The stack used by IRQ service routines.
//   SVC_STACK  -- The stack used in supervisor mode
//                 (Define other exception stacks as needed for
//                 FIQ, ABT, UND).
//   HEAP       -- The heap used by malloc and free in C and new and
//                 delete in C++.
//   INITTAB    -- Table containing addresses and sizes of segments that
//                 need to be initialized at startup (by cstartup).
//   CHECKSUM   -- The linker places checksum byte(s) in this segment,
//                 when the -J linker command line option is used.
//   DATA_y     -- Data objects.
//
// Where _y can be one of:
//
//   _AN        -- Holds uninitialized located objects, i.e. objects with
//                 an absolute location given by the @ operator or the
//                 #pragma location directive. Since these segments
//                 contain objects which already have a fixed address,
//                 they should not be mentioned in this linker command
//                 file.
//   _C         -- Constants (ROM).
//   _I         -- Initialized data (RAM).
//   _ID        -- The original content of _I (copied to _I by cstartup) (ROM).
//   _N         -- Uninitialized data (RAM).
//   _Z         -- Zero initialized data (RAM).
//
// Note:  Be sure to use end values for the defined address ranges.
//        Otherwise, the linker may allocate space outside the
//        intended memory range.
//*************************************************************************


//************************************************
// Inform the linker about the CPU family used.
//************************************************

-carm

//*************************************************************************
// Segment placement - General information
//
// All numbers in the segment placement command lines below are interpreted
// as hexadecimal unless they are immediately preceded by a '.', which
// denotes decimal notation.
//
// When specifying the segment placement using the -P instead of the -Z
// option, the linker is free to split each segment into its segment parts
// and randomly place these parts within the given ranges in order to
// achieve a more efficient memory usage. One disadvantage, however, is
// that it is not possible to find the start or end address (using
// the assembler operators .sfb./.sfe.) of a segment which has been split
// and reformed.
//
// When generating an output file which is to be used for programming
// external ROM/Flash devices, the -M linker option is very useful
// (see xlink.pdf for details).
//*************************************************************************


//*************************************************************************
// Read-only segments mapped to ROM.
//*************************************************************************

-DROMSTART=40000200
-DROMEND=40003FFF

//************************************************
// Address range for reset and exception
// vectors (INTVEC).
// The vector area is 32 bytes,
// an additional 32 bytes is allocated for the
// constant table used by ldr PC in cstartup.s79.
//************************************************

-Z(CODE)INTVEC=40000000-4000003F

//************************************************
// Startup code and exception routines (ICODE).
//************************************************

-Z(CODE)ICODE,DIFUNCT=ROMSTART-ROMEND
-Z(CODE)SWITAB=ROMSTART-ROMEND

//************************************************
// Code segments may be placed anywhere.
//************************************************

-Z(CODE)CODE=ROMSTART-ROMEND

//************************************************
// Original ROM location for __ramfunc code copied
// to and executed from RAM.
//************************************************

-Z(CONST)CODE_ID=ROMSTART-ROMEND

//************************************************
// Various constants and initializers.
//************************************************

-Z(CONST)INITTAB,DATA_ID,DATA_C=ROMSTART-ROMEND
-Z(CONST)CHECKSUM=ROMSTART-ROMEND

//*************************************************************************
// Read/write segments mapped to RAM.
//*************************************************************************

-DRAMSTART=40000200
//-DRAMSTART=40000000
-DRAMEND=40003EE0
//SM 40003FFF-120

//************************************************
// Data segments.
//************************************************

-Z(DATA)DATA_I,DATA_Z,DATA_N=RAMSTART-RAMEND

//************************************************
// __ramfunc code copied to and executed from RAM.
//************************************************

-Z(DATA)CODE_I=RAMSTART-RAMEND

//************************************************
// ICCARM produces code for __ramfunc functions in
// CODE_I segments. The -Q XLINK command line
// option redirects XLINK to emit the code in the
// CODE_ID segment instead, but to keep symbol and
// debug information associated with the CODE_I
// segment, where the code will execute.
//************************************************

-QCODE_I=CODE_ID

//*************************************************************************
// Stack and heap segments.
//*************************************************************************

//SM -D_CSTACK_SIZE=1000
-D_CSTACK_SIZE=100

// -D_SVC_STACK_SIZE=10
-D_IRQ_STACK_SIZE=200
-D_HEAP_SIZE=100

-Z(DATA)CSTACK+_CSTACK_SIZE=RAMSTART-RAMEND
// -Z(DATA)SVC_STACK+_SVC_STACK_SIZE=RAMSTART-RAMEND
-Z(DATA)IRQ_STACK+_IRQ_STACK_SIZE,HEAP+_HEAP_SIZE=RAMSTART-RAMEND

//*************************************************************************
// ELF/DWARF support.
//
// Uncomment the line "-Felf" below to generate ELF/DWARF output.
// Available format specifiers are:
//
//   "-yn": Suppress DWARF debug output
//   "-yp": Multiple ELF program sections
//   "-yas": Format suitable for debuggers from ARM Ltd (also sets -p flag)
//
// "-Felf" and the format specifiers can also be supplied directly as
// command line options, or selected from the Xlink Output tab in the
// IAR Embedded Workbench.
//*************************************************************************

// -Felf

Is it correct ? Cause my code doesn’t run well …

Thanks !