Reverse Engineering a Serial Communications Interaction

Hi. I’m hoping someone can help me solve a challenging problem or direct me to somewhere that might. I purchased a LIDAR module from a company called LeddarTech. The module works and communicates over a serial link via a USB port. It employs the MODBUS protocol. I’m trying to use a utility called ‘Device Monitoring Studio’ to examine the interaction between an executable provided by LeddarTech and the device in the hope that I can emulate the serial interaction between their executable and the device. DMS provides the following serial dump at the onset of communications with the device, which is a query for information about the identity of the device prior to configuration and use. I know the configurable name of the device is DEFAULT NAME. I know its serial number is AH48001. And both of those are apparent in the dump. Clearly, the dump must include data transmitted both to and from the device, but it is not clear from the dump where one ends and the other starts. Perhaps there is a better serial monitoring tool for my task that can differentiate the two? Can anyone offer any advice or insight as to how to proceed? Thanks so much.

http://www.afafa.org/LeddarTech_Modbus_Stream.png

Though I’ve never used any, there are hardware devices that can help with this. Here’s one:

https://www.stratusengineering.com/product/ez-tap-pro/