Hello. I have set up an automatic pet feeder with microview.
Since i had a pair of RF 433Mhz modules (one transmitter and one receiver) i’ve set up a raspberry pi i have as media center to send the updated time via RF to the pet feeder…
I have the microview feeded by a stripped usb cable on the VIN pin and i plug the RF module to the +5V pin of the microview.
The problem i have is that if i use poor/mid quality power sources (cheap cellphone chargers, <1A) the clock never updates, but if i use a very good and new cellphone charger (the one i use for my phone, ~2A) the clock updates with no problem… Also, if i plug the usb cable to my computer, it works ok too.
I have wired also to the VIN pin the servo motor, but while it updates the clock the servo doesn’t move…
my guess is that the voltage is too jumpy for the RF module to work correctly… but then i thought, surely the board has a power regulator for the +5V pin, right?
i haven’t tried yet to add a voltage regulator of my own, but it’s the next step i’m planning to take…
maybe you have a better idea of why this is happening?