RGB Matrix Controller

Anyone know what LED driver IC is used in the RGB controller? Its not marked on the schematics.

Thanks,

Vern

Judging from the diodes shown in the diagram, and something I read somewhere about it being a motor driver, I assume it is something similar to a [ULN2803 Darlington Array.](http://www.sparkfun.com/commerce/product_info.php?products_id=312)

Thanks lou, I am always interested in different ways to power bunches of LEDs.

Vern

Delicon,

Have you used this backpack controller yet? I bought 2 of them and having problems with a ghosted image offset of the text being sent across to it. Anything more than 64 bytes being sent to the controller causes this. I see this on 1 or 2 of them (cascaded DO to DI).

Have you seen this?

Well I found out that my problem with the ghosting was because of the microcontroller running faster than 125 KHz or so. I had it set to 4 MHz. However, now the scanning is so slow that it is nowhere’s near being “smooth” - refresh is very observable.

I set the DEVICE and FREQ as below:

DEVICE SX28, OSC128KHZ, TURBO, STACKX, OPTIONX

FREQ 128_000

Now what?

Hello,

Do you have this problem yet?

Unfortunately it gave me too many headaches and I did not want to invest any more time into that. Great display though. If you are using SX/B (BASIC) for a Parallax SX-28 or SX-48 micro-controller, I can email you what I originally wrote if you like.

gilmoret@us.saic.com

I’m using it with an arduino.

It works fine with my configuration:

i’m using a special firmware on my arduino + serial/OSC router + monome-like protocol

if you’re interested, i’ll post VERY soon my last release:

http://www.julienbayle.net/diy/LiveInterface/

it could be a way to control your matrix

I was posting that because I 'm hesitating with the serial router, cause of performance

  • w32 router (got the source, trying to change it) => works fine but only monochrome support

  • python router => rgb support, but little problem if i send A LOT of data very fast (I said VERY fast) but it works fine !

  • java router (I have to code it in processing ide)