I recently got an RN-41 module from sparkfun, and am having trouble getting it to do anything.
From the user guide, it appears I can simply connect it to a power supply (3.3V) and it will appear as discoverable by other bluetooth devices. However, it does not appear in my “bluetooth neighbourhood” or any other listings I can get under windows XP (I’m using a Belkin F8T013 USB adapter).
I’ve also tried connecting it to a serial interface, but don’t get any reply from the module (yes, I’ve set it to 115200 - N - 1).
At the bottom of the user guide it mentions that one of the hardware failure indications is a short between GND and Vcc. I get ~1k between those pins so I don’t believe this is the case, plus, I’m not using any of the IO pins (yet). I’ve had one of these modules working in the past, so this is baffling.
Does anyone out there have any ideas as to what this problem could be? What’s the chance the module is DOA?
Thanks, philip.