RN 52 SUPPORTING AT COMMANDS for COVERAGE AND QUALITY OF NETWORK

Hi,

I a working on a project where i need the support of AT commands, from which i can get the coverage (RSRP) and quality (RSRQ) of my connected phone’s network.

Below is an example : >>>

AT$QCRSRP Display Neighbor Cell Information RSRP (this is from AT&T_Commands_Guide_v1.7

Need the same for RN 52 .

For any help, thanks in advance

at.PNG

Hi diptesh.chakraborty,

I am not sure if the RN-52 is capable of getting those parameters. If it is, it would most likely be covered either in the [Datasheet or the [Command Reference User’s Guide. The RN-52 is primarily an audio module so it most likely does not have support for commands involving the network of an attached cellular device.](https://cdn.sparkfun.com/datasheets/Wireless/Bluetooth/rn-bt-audio-ug-2.0r.pdf)](https://cdn.sparkfun.com/datasheets/Wireless/Bluetooth/rn-52-ds-1.1r.pdf)

Thanks for your support TS-Mark.

I need this feature in my project. What can I do , either we need to develop the ROM or is there any other module available in which i can get these features ? , As my project really need this and required a bulk of RN-52.

We suggest you contact Microchip.

Microchip (formerly Roving Networks) make the RN-52 and should be able to tell you if the RN-52 has the capability of reporting RSRP and RSRQ. It’s possible that it may be supported with a firmware upgrade but Microchip will need to assist you with that.

You can visit the RN-52 page on the Microchip website at the link below.

  • https://www.microchip.com/wwwproducts/en/RN52