rn52 microphone

Hi… I have hooked up an rn52 and have it successfully streaming audio out via headphones or speakers. Now I want to attach a sound an Electret microphone part 09964 so I can use it as input.

The rn52 has mic r-, mic l-, mic +r, mic -r, m bias… while the electret microhpone only has aud, gnd, vcc… - so I figured just a mono connection - which would be fine…

So I hooked aud to mic -r and mic-+r, gnd to gnd, vcc to +3v.v.

Fire up the rn52 ---- and when I tap on the microphone I don’t hear anything…

Not sure what I have missed in the wiring — I have several other similar boards from adafruit and parallax - all doing the same thing… So I figure it is more in either the connection or an rn52 command I haven’t set.

Any help?

Microchip are launching a source mode version shortly. You are trying do do something not supported by the current profiles (A2DP, AVRCP, SPP)