Hi guys! ![]()
I’m working on a sensor system which should enable a robot arm to react as human activates a certain sensor.
So, what I have available is:
Capacitive sensor from Sparkfun: https://www.sparkfun.com/products/retired/9695
Proximity sensor from Adafruit: https://www.adafruit.com/product/466
Arduino UNO
Arduino ETHERNET SHIELD 2
Universal Robot UR5
So far my reach is connecting sensors to Arduino (I know, not much… I’m pretty new in all of this). The idea is to manipulate the robot by human hand, e.g. by touching conductive textile connected to MPR121 and mounted on the robot, it should stop/change direction, and by approaching with a hand to VCNL4010, it should slow down if in motion. The initial idea was to make it look like some sort of skin cell, but for now I would like to put these two sensors to work, and upgrade it step by step.
I’m aware of all the working principles of the Ethernet, but never actually dealt with it, or with Arduino contolled robot. So I’m wondering if anybody has some examples of similar projects or if anybody worked on something like that (Internet is full of everything, but when you need something specifically, it’s a blank page). At this moment I’m desperate because all my work comes down to brainstorming and wasting time.
What I made is the first version of a “skin cell”. Also, I have a problem with wires, not sure if i can connect multiple short wires to make a longer one since the proximity sensor should be on a robot arm with the conductive textile and Arduino itself somewhere around the base of the robot. I know resistance increases, and as a result, current decreases. I don’t know if I’m talking nonsense rn, but most of my knowledge is unfortunatelly theoretical.
Thank you advance! ![]()