Hai,
I have problem with rom debugging.
I burn appl.bin file, which is just simple led blink code. When i reboot the target, my application is running. When i tried to do romdebug, the insight windows shows the following
“Select function name to disassemble”
“Program stoped at 0x7fffd2b8”
My flash script file is as follows
arm7_9 dcc_downloads enable
wait_halt
sleep 10
poll
flash probe 0
flash erase 0 0 0
flash write 0 appl.bin 0x0
reset run
sleep 10
my gdb commands are as follows
target remote localhost:3333
monitor reset
monitor sleep 500
monitor poll
monitor soft_reset_halt
monitor arm7_9 hw_bkpts enable
break main
When i do single step, the openocd show following waring msg
"Info: arm7_9_common.c:277 arm7_9_add_breakpoint(): sw breakpoint requested, but software breakpoints not enabled
Info: breakpoints.c:73 breakpoint_add(): can’t add software breakpoint, resource not available"
Any help is highly appreciated
Karuna